Technical FAQs

Ask a Question

Is there a 90 degree connector available to connect to the motor lead terminals on the ATV340 series drives?

Issue:
Is there a 90 degree connector available to connect to the motor lead terminals on the ATV340 series drives?

Product Line:
ATV340 series drives

Environment:
All models, All serial numbers

Cause:
Information unavailable in current literature.

Resolution:
There currently is no option available for 90 degree connectors for the ATV340 series drives.

 

Was this helpful?
What can we do to improve the information ?