Technical FAQs

Ask a Question

What is the SCCR rating for the LS1D30 fuseholders?

 Issue:
Customer wants to know the Short Circuit Current Rating for the LS1D30

Product line:
LS1D

Environment:
n/a

Cause:
Not listed in the documentation

Resolution:
The label on the product states this is rated up to 200kA, 600VAC max and uses Class CC fuses.
 
Was this helpful?
What can we do to improve the information ?