Technical FAQs

Ask a Question

Do the 8501 Type X control relays meet IEEE 232 or IEEE 344?

 Issue:
Customer wants to confirm they can use the 8501X relays for applications that require IEEE approvals for IEEE 323-1983 and IEEE 344-1975

Product line:
8501X 8501XO 8501 Type X

Environment:
IEEE standards

Resolution:
The 8501 Type X relays do not meet either of these standards. 
Was this helpful?
What can we do to improve the information ?