Technical FAQs

Ask a Question

Do the GV2 enclosures carry UL50E Environmental ratings?

 Issue:
Customer wants to know if the GV2MP02 enclosure has UL50 protections.

Product line:
GV2

Environment:
n/a

Cause:
Documentation does not list.

Resolution:
The GV2 enclosures do not carry any UL enclosure ratings.  The GV2MP02 is IP55 rated. 

 
Was this helpful?
What can we do to improve the information ?