Technical FAQs

Ask a Question

Is 33185 a good number for a 24-30Vdc motor operator?

Issue:
How do you order 33185 24-30Vdc motor operator?

Product Line:
Masterpact Breaker

Environment:
Accessory for Masterpact NT Breaker

Resolution:
33815 is the motor operator component for 24-030Vdc Spring charging motor. Customer will need to order the complete spring charging motor kit, catalog number S47390.
Was this helpful?
What can we do to improve the information ?