Technical FAQs

Ask a Question

Is it possible to field install mod Z10 the service entrance ratings option on the ATS22 soft starter?

Issue:
Is it possible to field install mod Z10 the service entrance ratings option on the enclosed 22U ATS22 soft starter?

Product Line:
22U ATS22

Environment:
All 

Cause:
They forgot to order this mod when they bought the soft starter and want to add it in the field.

Resolution:
You will need to reach out to Seneca TAG to get the parts list and field services would need to install the parts. 
Was this helpful?
What can we do to improve the information ?