Technical FAQs

Ask a Question

What is the part number for the primary and secondary lug kits for a EX15T6HCT transformer?

Issue:
What is the part number for the lug kits for a EX15T6HCT?

Product Line:
Transformer

Environment:
EX Low Voltage Transformer

Resolution:
For the primary it is DASKP100 and the secondary it is DASKGS100
Was this helpful?
What can we do to improve the information ?