Technical FAQs

Ask a Question

What is "No Flow Fault" showing on the keypad of an ATV61?

 Issue:
What is "No Flow Fault" showing on the keypad of an ATV61?

Product Line:
Altivar ATV61

Environment:
All serial numbers

Cause:
Customer wanted to know what is the "No Flow Fault" showing on the keypad of his ATV61.

Resolution:
See the attachment for nFF or No Flow Fault from the ATV61 progamming manual. (https://www.schneider-electric.com/en/download/document/1760649/)

 
Was this helpful?
What can we do to improve the information ?