Technical FAQs

Ask a Question

Can an S-Flex be used to control an axial tube fan (turbine-style blade)?

Issue:
Can an S-Flex be used to control an axial tube fan (turbine-style blade)?

Product Line:
S-Flex enclosed drives

Environment:
All

Cause:
Customer has a turbine-style fan

Resolution:
Consult with your local Product Application Engineer to determine whether an S-Flex can be used on your particular application. 
This type of fan would draw more current than the regular-blade-type fan that the S-Flex's are designed for. It might work, but the drives would need to be derated.
For example: You may get a 50HP S-Flex to work on a 30HP fan, but we wouldn't recommend using a 50HP S-Flex on a 50HP turbine fan. 
 
Was this helpful?
What can we do to improve the information ?