Technical FAQs

Ask a Question

What is the calibration tool for a TK-1001 Thermostat?

Issue:
What does the TOOL-095-1 consists of?

Product Line: 
HVAC / Field Devices

Environment:
Actuator / Thermostat

Cause:
Calibration / Replacement / Maintenance

Resolution:

The calibration tool for the TK-1001 is part number TOOL-082. This is a combination 5/64" Allen Wrench, for Branch Test Port on Pneumatic Thermostats and Locking Cover Screws.
The other end of the Tool consists of a 0.048" , 6-spline Wrench for the Thermostat Calibration.

This can be purchased separately or within the calibration kit TOOL-095-1.

TOOL-095-1 consists of:
MCS-GA, N2-4, Female Branch Tee, TOOL-11, TOOL-78, TOOL-80, TOOL-82, TOOL-83, TOOL-87, TOOL-110,
AL-362 Air Line Tubing For Barbed Fitting, Air Line Tubing With Compression Fitting, 3/16 x 4" Blade Screwdriver
See attached 
Was this helpful?
What can we do to improve the information ?