Technical FAQs

Ask a Question

What is the bus rating for HOM2040M100PRB

Issue:
Is the bus rating for HOM2040M100PRB 100A or 125A?

Product Line:
Load centers
 
Environment:
Homeline Loadcenter, Nema 3R, 100A main breaker

Resolution:
HOM2040M100PRB has a  bus rating of 125A.  Information can be found on same label as wiring diagram.
Was this helpful?
What can we do to improve the information ?