Technical FAQs

Ask a Question

Is there a difference between an LP1D80008BD and an LC1D80FE7?

Issue:
What it the main difference between an LP1D80008BD and an LC1D80FE7?

Product Line: 
Tesys D line Contactors and Accessories

Environment:
IEC TeSys D Contactor Accessories

Resolution:
LP1 is a DC operated device and the LC1 is an AC operated device.  This LP1 is a 4 pole device and will not have hp ratings, the LC1 is a 3 pole device and will have HP ratings.  
Was this helpful?
What can we do to improve the information ?