Technical FAQs

Ask a Question

What is the breakout parts for a VK-7313-303-4-10 valve assy?

Issue:
What is the breakout parts for a VK-7313-303-4-10 valve assy? Lead time for assembly is too long , so ordering seperately preferred.

Product Line:
Valves and Actuators

Environment:
Product features

Cause:
Expedited shipment

Resolution:
The parts  are :
VB-7313-0-4-10 valve body
MK-4621 actuator 
AV-401 linkage
Was this helpful?
What can we do to improve the information ?