Technical FAQs

Ask a Question

What does "The module requires a voltage capacity that isn't available from the power supply" mean when I build my Unity project

Issue:
Unity gives the following warning message. "The module requires a voltage capacity that isn't available from the power supply"

Product line:
M340 M580 X80 Unity Pro

Resolution:
"The module requires a voltage capacity that isn't available from the power supply" warning message means the power supply does not provide a connection for sensor power.
 
Was this helpful?
What can we do to improve the information ?