Technical FAQs

Ask a Question

Failed loading translator DLL

Issue
All Micorlogic Trip units have stopped communicating in PME. The following errors can be seen in SystemLog:

          
          Transaction error. Device: 'SWBD_EDB.PNL_ELB_EHB'. Client: 'IONSERVICES.OHCOLAPP0999'. Reason: 'Failed loading translator DLL.'

Product Line
Power Monitoring Expert (any version)

Environment
Translator DLL file

Cause
The xlMicrologic.dll translator file is missing. It is suspected that an antivirus software has removed the DLL file.

Resolution
The DLL file should be located in .../System/Bin folder. First verify that the file is missing. Then download the attached file and drop it in the designated folder. Restart ION services.
Was this helpful?
What can we do to improve the information ?