Technical FAQs

Ask a Question

What are the termination sizes of the lugs for the Powerpact B frame circuit breaker?

 Issue:
What are the wires sizes for the lugs on the Powerpact B frame circuit breaker?

Product Line:
Powerpact B frame circuit breakers.

Environment:
Molded Case Circuit Breakers.

Cause:
Wires sizes and terminations needed for lugs for a Powerpact B frame circuit breaker.

Resolution:
Wires sizes may be found in the current on line digest https://www.productinfo.schneider-electric.com/portals/ui/digest/viewer/561d5d65e4b0c5c41a243bf2/561d5f9ae4b0c5c41a24480c/r/_17707042_30026#_17707042_30026
Was this helpful?
What can we do to improve the information ?