Technical FAQs

Ask a Question

How can an MP-371 receive a 0-10 vdc control signal?

Issue:
How can an MP-371 actuator, which has 2-12 vdc input signal range, receive a 0-10 vdc control signal?

Product Line: 
Valves and Actuator

Environment:
Maintenance / Installation / Set-up

Cause:
Product Characteristics / Application assistance

Resolution:
In order to make the actuator receive a different control signal , rather than it's factory configuration, in this case 2-12 VDC, the use of an actuator drive kit , which can remedy the input DC voltage differences.
For an MP-371 Actuator, which has 2-12 vdc input signal, can use the CP-9301-456 drive kit, see instuction bulletin below 
 
Was this helpful?
What can we do to improve the information ?