Technical FAQs

Ask a Question

How does an MA-418-500 differ from an MA-418?

Issue:
How does an MA-418-500 Actuator differ from the MA-418 actuator ?

Product Line: 
Valves and Actuator

Environment:
Application

Cause:
Product Features

Resolution:
The difference between an MA-418-500 Actuator and the MA-418 Actuator is the addition of an auxiliary switch attached (-500) to the actuator and cannot be added in the Field . Both Actutaors have the same functionality
(MA-418-500) has aux switch
(MA-418) no aux switch
 
Was this helpful?
What can we do to improve the information ?