Technical FAQs

Ask a Question

Can I have multiple Battery Monitors connected to my battery bank?

Issue:
Can I have multiple Battery Monitors connected to my battery bank?

Product Line:
Conext Battery Monitor

Environment:
Large Battery bank with multiple strings.

Cause:
Battery Backup system can only have as many battery banks as it has Inverters.

Resolution:
Parallel the Battery bank so that you only need one Battery Monitor for the system. If a larger shunt is needed, change shunt resistor and adjust settings on BMS.
If there are multiple inverters in the system and multiple battery monitors are to be installed, make sure to use separate battery banks for each inverter.
Was this helpful?
What can we do to improve the information ?