Technical FAQs

Ask a Question

What is the conduit kit for ATV320U55S6C?

Issue:
Looking for the accessory that attaches to the lower part of the drive to allow direct connection of cables

Environment:
Altivar 320

Product Line:
Variable Frequency Drives

Cause:
Wall mounted drive that requires a kit to connect the wires via tubes or cable glands

Resolution:
The UL type 1 conformity kit or the conduit kit is VW3A95816

Keywords:
Conduit kit, conformity kit, ATV320, wall-mount
Was this helpful?
What can we do to improve the information ?