Technical FAQs

Ask a Question

XW giving AI fault within AC Input Setting Ranges

Issue:
Why is my XW giving me AI faults even though my AC settings have higher voltages?

Product Line:
Conext XW+

Environment:
XW inverter showing Anti-Islanding fault while grid voltage is within AC Settings range.

Cause:
When Grid Support function is Enabled AC Input Settings  limits are overridden by the default anti-islanding AC parameters.

Resolution:
See Anti-Islanding allowed ranged in the picture attached. Table can also be found on the Owner's Manual (Link Below) page A-3 or PDF page 127.

https://41j5tc3akbrn3uezx5av0jj1bgm-wpengine.netdna-ssl.com/wp-content/uploads/2018/01/ML201711_Conext-XW-NA-Owners-Guide-975-0240-01-01_Rev-H_ENG.pdf
Was this helpful?
What can we do to improve the information ?