Technical FAQs

Ask a Question

video: How to check and change the port in AOA?

To execute the runtime of Ecostruxure Augmented Operator Advisor (AOA), some port have to be open and free
Here the list of port used by AOA
- 80     : Augmented Operator Advisor http (nginx)
- 443  : Augmented Operator Advisor https (nginx)
- 8082 : Augmented Operator Advisor WEB services (python)
- 8080 : Vijeo XD variables access (pcplatform)
- 1882 : Node-RED SQL variables (node)

In case of port conflict, some trouble can occur (No connection with the server, Variable from VXD not working etc etc)
The following video explain how to check the port and change it properly

https://youtu.be/zhYKB_SrqNg

Was this helpful?
What can we do to improve the information ?