Technical FAQs

Ask a Question

What is the adapter kit/ linkage for a Forta M400A, M800A actuator with a VB-7XXX Series valve ?

Issue:
What is the adapter kit/ linkage for a Forta M400A, M800A actuator with a VB-7XXX Series valve ?

Product Line:
Valves and Actuators

Environment:
Installation

Cause:
Compatibility

Resolution:
The AV-821 Adaptor is needed to connect the valve shaft and Forta actuator's U Bolt collar.
  Forta Actuator with  VB-7XXX valveAV-821 Adaptor

See Attached Data sheet for Adaptor 
Was this helpful?
What can we do to improve the information ?