Technical FAQs

Ask a Question

What is the part number of RC circuit coil suppressor for a 60…120V LC1D09 to LC1D38 contactor

Issue:
Is there a suppressor module for LC1D09 to LC1D38 contactors?

Product Line:
IEC TeSys D Contactors

Environment:
TeSys D control relays Add-on blocks
 
Resolution:
LAD4RCG is the suppressor module that clips onto the top of the control relay and the electrical connection of an LC1D09 to LC1D38.
Was this helpful?
What can we do to improve the information ?