Technical FAQs

Ask a Question

Can I use a control circuit voltage that's outside the recommended range with an ATS22 Soft Starter?

Issue:
Can I use a control circuit voltage that's outside the recommended range with an ATS22 Soft Starter?

Product Line:
Altistart 22

Environment:
All

Cause:
Customer has different (higher or lower) voltage available and wants to use it

Resolution:
No, we do not recommend using control voltage that is outside the recommended range listed in the Installation Manual. Anything outside the recommended range for the Soft Starter's control voltage may cause damage to the drive. 
The control voltage needed depends on the Soft Starter's part number. We only recommend a range of +10% and -15% of the applicable voltage rating. 
Please reference the ATS22 Installation Manual for further details. 

Was this helpful?
What can we do to improve the information ?