Technical FAQs

Ask a Question

What is the AIC rating for FJA14040?

Issue:
What is the interrupting rating for FJ breakers at 240Vac?

Product Line:
Molded Case Circuit Breakers

Environment:
F Frame Molded Case Breakers

Resolution:
The FJ breaker is rated 65kA@240Vac. It can be used at the maximum voltage of 277Vac and the interrupting rating is also 65kA.
Was this helpful?
What can we do to improve the information ?