Technical FAQs

Ask a Question

What does "3" stands for on XD4PA223?

Issue:
Joystick Connection

Product Line:
22 mm Push Buttons

Environment:
XB4 Specialty Operators

Resolution:
XD4PA**3 means it uses a faston connector. Part# without the #3 suffix is a screw termination.
Was this helpful?
What can we do to improve the information ?