Technical FAQs

Ask a Question

Is there a way to calculate the minimum current entered to nCr parameter in ATV320 drive?

 Issue:
Is there a way to calculate the minimum current entered to nCr parameter in ATV320 drive?

Product Line:
Altivar 320, ATV320

Environment:
All serial numbers, all model numbers

Cause:
Customer tried to set 1.5A in the nCr parameter but the drive wouldn't take lower than 2A.

Resolution:
2A is the minimum rate motor current that the customer can enter into the drive.  It is calculated by taking nominal current * 0.25 which is 8*.25=2A.
Was this helpful?
What can we do to improve the information ?