Technical FAQs

Ask a Question

Are the Powerpact B-frames switch duty rated?

Issue:
Do the B-frame circuit breakers carry a switch duty rating?

Product Line:
Molded Case Circuit Breakers

Environment:
B-Frame Circuit Breakers

Resolution:

The 15 A and 20 A B-frames (1p, 2p, and 3p) are switch duty rated when applied at 347 V or less.
Was this helpful?
What can we do to improve the information ?