Technical FAQs

Ask a Question

What is then difference between the ME-12313-100 and ME-12313 actuators , are they still available?

Issue:
Trying to find a Actuator that was obsoleted , what is the difference bertween the obsoleted ME-12313-100 actuator and the Invensys ME-12313 Actuator ?

Product Line:
Valves and Actuators 

Environment:
Maintenance 

Cause:
Prioduct Features

Resolution:
The ME12313 is obsolete with no replacement, whereas the ME-12313-100 actuator had a Square output shaft and a different package kit included. This is Actuator is also obsolete with no replacement.
Was this helpful?
What can we do to improve the information ?