Technical FAQs

Ask a Question

Where to get 1070-C Low Voltage Relay?

Issue:
Low Voltage Lighting Relay

Product Line:
Square D Telemecanique Relay

Environment:
North American Products

Resolution:
Where Used:
Unique low voltage remote control system which provided a convenient means of adequately switching lighting and appliance circuits in homes, office buildings, industrial plants, schools, churches, warehouses and many other applications.
These units were marketed during the 50's and early 60's by the Distribution Division (Lexington).
Part Status:
Obsolete - Product line sold.

Replacement Information
Contact the following company for replacement parts/retrofit information.

Pass & Seymour / Legrand
Syracuse, NY  (315)468-6211
Was this helpful?
What can we do to improve the information ?