Technical FAQs

Ask a Question

What is the bus rating for HOM4080M200PC?

Issue:
Does HOM4080M200PC have a bus bar rating of 225A?

Product Line:
Load Center

Environment:
PON Homeline Load Center

Resolution: 
The mains rating is 200A, bus bar rating is 225A.  This is noted on the Box Label located on the inside wall of the enclosure.
Was this helpful?
What can we do to improve the information ?