Technical FAQs

Ask a Question

What is the Short Circuit Current Ratings of part number CA2KN40G7?

Issue:
Do relays have Short Circuit Current Ratings?

Product Line:
Tesys K IEC Style Relays

Environment:
Relays and Timers

Resolution:
Relays have no Short Circuit Current Ratings. Only circuit breakers, disconnects and contactors have Short Circuit Current Ratings. Relays are used in the control circuit . Only the power circuits have SCCR
Was this helpful?
What can we do to improve the information ?