What does the C stand for at the end of the catalog number QO1515C
Answer
Issue:
Product Selection Features
Product Line:
QO Load Centers
Environment:
Selection of tandem breakers
Cause:
Selection
Resolution:
The C at the end of QO1515C represents consumer packaging. In this case it is a plastic clam shell type of packaging.
QO1515 can be ordered as standard, shipped in boxes of ten pcs