Technical FAQs

Ask a Question

Can the MK-6811 actuator work with the VB-7XXX Valves, it was used with a VB-9XXX valve before? VB-7223-0-4-09 Valve for example

Issue:
Can the MK-6811 actuator work with the VB-7XXX Valves, it was used with a VB-9XXX valve before?

Product Line:
Valves and Actuators

Environment:
Maintenance 

Cause:
Replacement 

Resolution:
The MK-68XX Series actuators wwere used with the old VB-9XXX Series of valves and will NOT work with new VB-7XXX series valves.
For the VB-7223-0-4-09 Valve , the recommendation would be to use a MK-661 actuator with AV-430 linkage.
Was this helpful?
What can we do to improve the information ?