Technical FAQs

Ask a Question

Column EQUIP is not found

Issue
When removing a device from a project, the following error appears:



Failed to remove the profile instance from your project. Your project may have been modified. It is recommended that you restore it from a recent.
Error: An error occurred while deleting a row from 'events.DBF'. Details:
SQL: Column 'EQUIP' is not found.


Product Line
PowerSCADA Expert 8.2

Environment
I/O Device Manager

Cause
Trying to remove a device from the project.

Resolution
The events.DBF file was missing a few columns, one being the EQUIP column. As such, the file needs to be replaced by one from a working system (same version). The following columns should exist:
NAME, TIME, PERIOD, TRIG, EVENT, COMMENT, CLUSTER, EQUIP, EDITCODE, LINKED, TAGGENLINK
Was this helpful?
What can we do to improve the information ?