Browse FAQs

Can a QO-VH breaker be use in the QO OEM mounting bases?

Published date: 27 August 2019

Issue:
Can a QO270VH be used in QON2L70 ?
 
Product Line:
Miniature Circuit breaker
 
Environment:
QO Circuit Breakers, QO OEM mounting base
 
Resolution:
No. QO OEM mounting bases are 10k AIC rated and the VH suffix indicates a 22k AIC rating.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.