Technical FAQs

Ask a Question

How can your read the drives thermal in percent on the ATV212 and S-Flex drives display ?

Issue:
How can your read the drives thermal in percent on the ATV212 and S-Flex drive?

Product Line:
ATV212 and S-Flex

Environment:
All 

Cause:
Wants to read the drives thermal to see how hot its getting

Resolution:
You can change the default keypad operational value by changing F710 to 4 (Drive controller thermal state %)
Programming
Mode to AUF arrow down to F------- enter
Arrow down to F710 enter 
Change F710 to 4 enter. 
Done
Was this helpful?
What can we do to improve the information ?