Technical FAQs

Ask a Question

What are the available shunt trip for the TeSys GV7 Manual Starters?

Issue:
What is the part number of the GV7 shunt trip?

Product Line:
IEC TeSys GV7 Manual Starters and Protectors

Environment:
IEC TeSys GV7 Manual Starters and Protectors sold and used in the United States
 
Resolution:
There should be 1 shunt trip per device depending on the voltage range and is mounted inside. Refer to table below for selection.
Voltage Catalog Number
48 Vac 50 Hz  GV7AS055
110-130 Vac 50/60 Hz  GV7AS107
200-240 Vac 50/60 Hz  GV7AS207
380-440/480 Vac 50/60 Hz  GV7AS387
525 Vac 50 Hz  GV7AS525






 
Was this helpful?
What can we do to improve the information ?