Technical FAQs

Ask a Question

What are the default presets for my Battery Type?

Issue:
How do I know when I need to use a Custom battery type in my SCP or Combox?

Product Line:
MPPT60, MPPT80, Conext SW, Conext XW+, System Control Panel, Combox

Environment:
Initial commissioning, or installation of new batteries with any Conext System

Resolution:
  Flooded AGM Gel Lithium Ion
Equalization 64.0 n/a n/a n/a
Bulk 57.6 57.2 56.8 57.0
Absorption 57.6 57.2 56.8 58.0
Float 54.0 53.6 55.2 53.6
*For 24V, divide values by a factor of 2

Cause:
Battery manufacturers will often give specific values for charging that will differ from our presets.
Was this helpful?
What can we do to improve the information ?