Technical FAQs

Ask a Question

How do you wire a transducer for 4-20mA on the ATV312 drives?

 Issue:
Customer wired ATV312 with AI3 and COM but the drive is not responding to the 4-20mA signal.

Product line:
ATV312, Altivar 312

Environment:
all

Cause:
Wiring

Resolution:
2 wire transducers need to have a power supply.  Connect the Negative or Common wire from the transducer to the 24V terminal.  The output or Positive will land on AI3 terminal. 

 
Was this helpful?
What can we do to improve the information ?