Technical FAQs

Ask a Question

Is there an adjustable roller lever for the L100/L300 Limit Switch?

Issue:
What is the part number of the adjustable roller lever for the L100/L300 Limit Switch?

Product Line:
L100/300 Limit Switch

Environment:
L100/300 Accessories
 
Resolution:
AL2820 is a Roller, Adjustable from 2 to 4 in. (0.25 in. wide, 0.75 in. diameter) for L100/L300 Limit Switch.
Was this helpful?
What can we do to improve the information ?