Technical FAQs

Ask a Question

Video: What is the default grid snap setting in Vijeo Designer v6.2?

The default spacing is 20x20 pixels.  It can also be changed from the Graphical Panels Properties.

The following video demonstrates adjusting the grid snap spacing in Vijeo Designer via the Graphical Panels Property Inspector.

 
Was this helpful?
What can we do to improve the information ?