Technical FAQs

Ask a Question

:CBUS: Can you operate the 5500shac network directly from the 5000EPT10W touchscreen?

Yes, using either crossover or straight through network cable

Touchsrcreen need to be on the same IP range as the Shac/Nac
 

 

Was this helpful?
What can we do to improve the information ?