Technical FAQs

Ask a Question

What type of transformers replace the old EP premium transformers?

Issue:
What is the current style transformer that replaces the 3 phase EP transformers?

Product Line:
General Purpose Type Transformer

Environment:
EX Transformers

Cause:
Installation

Resolution:
The old EP type 3 phase transformers have been replaced with the current style EX transformers that meet the DOE 2016 requirements.
Was this helpful?
What can we do to improve the information ?