Technical FAQs

Ask a Question

Are retrofit kits available for Schneider Electric actuator to fit in for a Honeywell valve VP519C?

Are there Schneider Electric actuator retrofit kits available to fit a Honeywell valve VP519C?

Product Line: 
Valves and Actuator


Retrofit / Replacement

There are no retrofit kits available for our actuators to fit in for a Honeywell valve VP519C. The VP519C is a pneumatic air valve which is closely similar to our AL-161-4, but the AL-161-4 is a pneumatic package which means they can't just change out the actuator to Schneider's . Honeywell  Valve and Actuator will both need to be replaced .
Was this helpful?
What can we do to improve the information ?