Technical FAQs

Ask a Question

Can I change the LXM28 speed on the fly using MC_MoveVelocity?

Issue:
Can I change the LXM28 speed on the fly using MC_MoveVelocity?

Product Line:
LXM28

Resolution:
Unfortunately, this is not possible without a toggle on the Execute pin.
Please see attached workaround.
Was this helpful?
What can we do to improve the information ?