Technical FAQs

Ask a Question

Do we have a 9007C that is Nema 4x and Nema 7 rated limit switch?

Issue:
Do we have a 9007C that is Nema 4x and Nema 7 rated limit switch?

Product Line: 
Limit Switch

Environment:
North American Products

Cause:
Do we have a 9007C that is Nema 4x and 

Nema 7 rated limit switch?

Resolution:
No, For our 9007C Limit Switches is only rated for NEMA Types 2, 4, 6, 6P, 12, 13 see page 21-3 Digest 177 and see Table 21.1: Enclosure Ratings on page 21-4 (attached) 
Was this helpful?
What can we do to improve the information ?