Technical FAQs

Ask a Question

What would cause a code 50 on an ATV312?

Issue:
What would cause a code 50 on an ATV312?

Product Line:
Altivar 312

Environment:
All

Cause:
Seeing '50' on the face of the drive

Resolution:
'50' is not a valid fault code. It's possible that you're seeing the current speed that the drive is running (50Hz). 



 
Was this helpful?
What can we do to improve the information ?