Technical FAQs

Ask a Question

What is the part number for the GT Modbus copper connection cable that connects to the CCU board connection J1004?

Issue:
Part Number validation for the modbus copper connection

Product Line:
GT100, GT250

Environment:
Applications that use the 3phase utility scale unit such as the GT100 or GT250 units

Cause:
Determining the Modbus copper connection kit part number for ordering or installing

Resolution:
The part# is 1-153481-01 (or 0W-153481-01)
The part can also be ordered as part of the whole kit: 0J-0N-153482-01

Was this helpful?
What can we do to improve the information ?